Visitez notre boutique en ligne MISUMI et découvrez un grand choix de pièces standard configurables.
Découvrir maintenant
Surface Treatment

Order your Finished Milled Parts

Here you will find details of the options for finishing your parts with meviy. Take a look at our available surface treatments in detail and convince yourself of our quality.

Get an instant quote
Example of a milled part manufactured with meviy.

Surface Treatments

The treatment of surfaces plays an essential role in various industrial sectors, as it represents a decisive step in improving the performance, durability and visual appeal of materials. From the finishing of metals to the coating of plastics, surface treatments offer a wide range of processes aimed at specifically modifying and optimising the properties of surfaces.

Here we present a comprehensive overview of all available surface treatments from meviy. Our diverse techniques and processes not only open up the possibility of making materials more aesthetically pleasing, but also improve their functionality and durability. Discover the numerous surface treatment options and find the optimum solution for your individual requirements and applications.

Black Oxide
Black oxide coating, which creates a thin, corrosion-resistant layer on the material and is often used in the automotive industry, mechanical engineering and precision mechanics.
Electroless Nickel Plating
Electroless nickel plating, which offers excellent corrosion protection and a uniform coating and is often used in electronics, the automotive industry and mechanical engineering.
Hard Chrome Plating
Hard chrome plating (short-term chrome plating), which provides a hard, wear-resistant surface with excellent corrosion resistance and is used in the aerospace, hydraulics and tool industries.
Trivalent Crhomated (Clear)
The chromated (III-valent) coating (clear), which improves the corrosion resistance of aluminium surfaces and can serve as a primer for paints and varnishes, and is often used in the aviation, electronics and automotive industries.
Trivalent Crhomated (Black)
The trivalent chromate coating (black), which offers similar advantages to the clear chromate coating, but with a dark, decorative surface, and is often used in the electronics, defense and automotive industries.
Anodised (Clear)
The clear anodised coating that provides excellent corrosion protection for aluminium surfaces and is used in architecture, electronics and mechanical engineering.
Anodised (Black)
The black anodised coating, which offers similar advantages to the clear anodised coating, but with a dark, decorative surface, and is often used in the aviation, electronics and automotive industries.
Black Anodised (Matt)
The black anodised coating (matt), which provides a matt, black surface with excellent corrosion and abrasion resistance and is often used in the electronics, furniture and design industries.
Anodised (Red)
The red anodised coating, which offers similar advantages to the clear anodised coating, but with a red, decorative surface, and is often used in the electronics and automotive industries.
Anodised (Gold)
The gold anodised coating, which offers similar advantages to the clear anodised coating, but with a golden, decorative surface, and is often used in electronics and jewellery manufacture.